IMX8 clock in int1177

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 clock in int1177

699 Views
khaledbalbaa
Contributor I
I am trying to output a 25MHz clock on pin MIPI_CSI0_MCLK_OUT on imx8 B0 board int1177
But unfortunately I don't know the name of the clock that I can use on this pin neither the frequency values that I can output
Could you please tell me how to find the name of the clock to use it in the Device tree or in the SCFW APIs?
Also I would like to know if this clock has a fixed frequency value or I can configure it, and what are the values that I can use
Tags (2)
0 Kudos
Reply
1 Reply

557 Views
igorpadykov
NXP Employee
NXP Employee

Hi Khaled

this pin is directly connected to the 24MHz reference clock used in the
MIPI-CSI2 IP. There is no possibility to change the frequency.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply