Board Type: NXP i.MX8MNano LPDDR4 EVK board
Why does UUU qspi write to flash not result in U-boot running with correct boot settings and powered ON? See Test 1 below. The same process works successfully when using eMMC storage.
Note that also I tried the UUU "nand" option, but UUU fails.
Test 1 (qspi):
##############
Power OFF.
Set boot switch to Download Mode.
Power ON
Issue uuu.exe command (Windows 11 Powershell).
PS D:\downloads\uuu_source-1.4.243> ./uuu.exe -b qspi imx8-boot-sd.bin
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51
Success 1 Failure 0
2:13 9/ 9 [Done ] FB: done
Power OFF
Set boot switch to NAND Flash.
Power ON
Nothing occurs.
Test 2 (emmc):
##############
Power OFF.
Set boot switch to Download Mode.
Power ON
Issue uuu.exe command (Windows 11 Powershell).
PS D:\downloads\uuu_source-1.4.243> ./uuu.exe -b emmc imx8-boot-sd.bin
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51
Success 1 Failure 0
2:13 7/ 7 [Done ] FB: Done
Power OFF
Set boot switch to eMMC.
Power ON.
U-Boot starts as expected with my U-Boot Version.
解決済! 解決策の投稿を見る。
Hello,
I notice that you’re actually using the wrong binary since you’re trying to flash an SD boot image instead of one for Flexspi.
You may download the demo image and try with that, by using the following command:
./uuu.exe -b qspi imx-boot-imx8mnevk-fspi.bin-flash_evk_flexspi
Demo image is available for download here:
https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...
Best regards,
Aldo.
Aldo,
That was the information I needed!
Thanks,
John
Aldo,
I tried both the settings for "QSPI 3B Read" and "QSPI Hyperflash 3.3V" boot selections. In neither case does the i.MX 8M Nano LPDRR4 EVK boot. As stated initially, the uuu command reports success when targeting QSPI, but fails to boot. When targeting eMMC memory - uuu reports success and the board boots.
Thanks for your prompt response,
John
Hello,
I notice that you’re actually using the wrong binary since you’re trying to flash an SD boot image instead of one for Flexspi.
You may download the demo image and try with that, by using the following command:
./uuu.exe -b qspi imx-boot-imx8mnevk-fspi.bin-flash_evk_flexspi
Demo image is available for download here:
https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...
Best regards,
Aldo.
Hello,
Please note that you're actually flashing the MT25QU256ABA1EW, the QSPI memory is connected to the FlexSPI interface of i.MX 8M Nano LPDRR4 EVK, so you'll need to set switches to boot from QSPI not NAND.
Please refer to the following document on how to set the dip switch, chapter 2.2 Boot mode and boot device configurations:
https://www.nxp.com/webapp/Download?colCode=IMX8MNLPD4EVKHUG
Best regards,
Aldo.