On the imx7d dev board, there is an EPD connector J13 that has i2c, interrupt, which seems like I could customize the device tree to talk to touch panels with a common FT5x16 6 pin interface. Seems overkill though to buy a 120 pin connector and use 6 of them. Is there a better way to bring those signals in and customize them during development?
I thought of using the I2C pins connected to the LCD 50 pin connector but there doesn't seem to be any pin available I could use as the interrupt. Anyone have a better way to solve this or is using J13 the best way to go?
Hi Dennis
seems you are right: spi signals on J14 connector (38..41) i.MX7D Sabre SD
can be configured as gpios and used as interrupt sources.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for the follow up. Can any GPIO be used as an interrupt or do I have to stick to the SPI pins? I have other peripherals to add and configure as I start work on this so eventually I'll need to reuse quite a few of the pins in that connector although I don't yet know how many need interrupt abilities.
Hi Dennis
yes any GPIO can be used as an interrupt.
Best regards
igor