IMX7D USB_OTG_VBUS allowed enable power level?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7D USB_OTG_VBUS allowed enable power level?

Jump to solution
977 Views
frankyhsu
Contributor III

Hi Support,

We are checking the property of this pin and we might need to use 3.3V instead of 5V from USB connector. What's the limitation? Is 3.3V of for it?

Labels (1)
0 Kudos
Reply
1 Solution
707 Views
Yuri
NXP Employee
NXP Employee

Hello,

  In order to meet specs, minimum VBUS is 4.75 V; maximum is 5.25V.

 Generally, i.MX7 can work in device mode without VBUS, but it is needed to modify

software to disable VBUS detection.

   But the following impacts should be taken in consideration:

 1) i.MX7 may NOT detect plug in/out events, because the interrupt is triggered

  by the VBUS level;

2) i.MX7 USB may NOT work at low power mode, because VBUS functions as the

  wake-up source.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

https://community.nxp.com/message/586582 

View solution in original post

0 Kudos
Reply
3 Replies
708 Views
Yuri
NXP Employee
NXP Employee

Hello,

  In order to meet specs, minimum VBUS is 4.75 V; maximum is 5.25V.

 Generally, i.MX7 can work in device mode without VBUS, but it is needed to modify

software to disable VBUS detection.

   But the following impacts should be taken in consideration:

 1) i.MX7 may NOT detect plug in/out events, because the interrupt is triggered

  by the VBUS level;

2) i.MX7 USB may NOT work at low power mode, because VBUS functions as the

  wake-up source.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

https://community.nxp.com/message/586582 

0 Kudos
Reply
707 Views
frankyhsu
Contributor III

We see that the 3.3V input and even lower to 1.8V, it can still work

unless we connect nothing. So, NXP can still accept the 4.75 as the

minimum?

Franky Hsu

Sercomm Corp.

2F, No.3-1, YuanQu St., Nankang, Taipei 115, Taiwan

+886-2-26553988 #2552

寄件者: "Yuri" <admin@community.nxp.com>

收件者: "Franky Hsu" <franky_hsu@sercomm.com>,

日期: 2017/12/14 下午 12:04

主旨: Re: - Re: IMX7D USB_OTG_VBUS allowed enable power

level?

NXP Community

Re: IMX7D USB_OTG_VBUS allowed enable power level?

reply from Yuri Muhin in i.MX Community - View the full discussion

Hello,

In order to meet specs, minimum VBUS is 4.75 V; maximum is 5.25V.

Generally, i.MX7 can work in device mode without VBUS, but it is needed

to modify

software to disable VBUS detection.

But the following impacts should be taken in consideration:

1) i.MX7 may NOT detect plug in/out events, because the interrupt is

triggered

by the VBUS level;

2) i.MX7 USB may NOT work at low power mode, because VBUS functions as the

wake-up source.

Have a great day,

Yuri

0 Kudos
Reply
707 Views
Yuri
NXP Employee
NXP Employee

Hello,

   You may use Your configuration - it does not violate (hardware) maximum ratings,

but do not forget about possible (software) impacts. 

Regards,

Yuri.

0 Kudos
Reply