IMX7D SAI interface - rx delay

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX7D SAI interface - rx delay

ソリューションへジャンプ
2,198件の閲覧回数
aswinmohan
Contributor I

Hi,

I am using IMX7D SAI interface in master, synchronous mode.

It is configured to send /receive MSB first.

The slave device is able to receive the data, TX from SAI, properly.

But while sending, it is having a delay of 2 clock cycles.

Is there a way to delay the RX word sampling start, by 2 clock cycles (from start of frame), in SAI.

Thank you

Aswin

ラベル(2)
0 件の賞賛
返信
1 解決策
2,023件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aswin

it is possible to delay the RX word sampling by one clock using bit

FSE register I2Sx_RCR, but seems there is no option to delay for two clocks.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,024件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aswin

it is possible to delay the RX word sampling by one clock using bit

FSE register I2Sx_RCR, but seems there is no option to delay for two clocks.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,023件の閲覧回数
aswinmohan
Contributor I

Thank you Igor

0 件の賞賛
返信