Hi Franky
if M4 performing some interaction with WiFi module or other activity,
then it can not be put in low power mode. Driver implementation can be
found in sect.4.12 Wi-FI BCM4339 attached Linux Manual. Also as described
in Table 5-5. Low Power Mode Definition i.MX7D Reference Manual
http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf
M4 (it is in SOC power domain) can be ON/Clock Gated or OFF in lowe power
modes, there are no other options.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------