Hi,
We are planning to use IMX7D because of the heterogeneous architecture in which DDR RAM is shared between the two cores, and can achieve the best speed across the M4 and A7 communication.
We have seen some threads to identify communication between A7 and the M4 core using RPMSG but not sure about the throughput of that. Basically we are targeting 5 to 7 Mbps transfer between the core.
We are planing to follow below approaches to achieve this,
We are aware about that DDR RAM is single reader and single writer from M4 and A7. So, only one can access it at a time.
Can we achieve high data transfer from M4 to A7 in anyway by taking advantage of shared memory ?
Hi Nilesh
>Can we achieve high data transfer from M4 to A7 in anyway by taking advantage
>of shared memory ?
in general yes, 5 to 7 Mbps transfer between the cores may be feasible.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Nilesh
one can look at shared memory example in
FreeRTOS_BSP_1.0.1_iMX7D/middleware/multicore/open-amp/rpmsg/rpmsg_rtos.c
and optimize it for own needs:
FreeRTOS_iMX7D_1.0.1_WIN
Best regards
igor