IMX7 industrial grade?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7 industrial grade?

949 Views
kerkchoonhuei
Contributor I


Is I.MX7 available on industrial grade?

It is listed in datasheet as industrial grade, but from the NXP website sample and buy under "Qualification Tier" it is listed as 5-years application life which is consumer applications.

E.g.:

MCIMX7D3EVK10SC & MCIMC7D5EVM10SC are both listed as industrial grade in the datasheet, but it is listed as 5-years application life typically for consumer application.

So are the above-mentioned 2 parts industrial grade?

Labels (1)
0 Kudos
3 Replies

699 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the data sheet, MCIMX7D3EVK10SC & MCIMC7D5EVM10SC are both listed as industrial grade, and Industrial qualification grade assumes 10-year lifetime with 100% duty cycle.

0 Kudos

698 Views
SKWoon
NXP Employee
NXP Employee

I think he is referring to the "Buy" tab on nxp.com, refer to below link & attached screenshot which states "5-YEARS APPLICATION LIFE":

i.MX 7Dual Arm Cortex-A7 Processor|NXP

0 Kudos

698 Views
kerkchoonhuei
Contributor I

Thanks Sock Keng.

That is correct. There seems to be conflicting information comparing datasheet and online information.

Need help to verify. Thanks.

0 Kudos