IMX7 ULP can't connect to Serial Download Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7 ULP can't connect to Serial Download Mode

453 Views
EngineerPMIC
Contributor I

Hi,

I am working on a design with the IMX7ULP. By default BOOTMODE_1 and BOOTMODE_0 are pulled down to ground so the boot type is Boot from Fuses. After the eMMC is flashed I want to get this to Serial Download mode so I can update the image. So when I change BOOTMODE_1 and BOOTMODE_1 to 01 it never enters Serial Download mode. It looks like it is hanging somewhere. When change the bootmode pins back to 00 the device starts booting from the eMMC. Can someone help me figure out what is going wrong?

 

Labels (1)
0 Kudos
1 Reply

441 Views
joanxie
NXP TechSupport
NXP TechSupport

pls check the BT_FUSE_SEL bit, refer to the Table 35-4. i.MX 7ULP boot modes of reference manual, Boot Configuration is loaded from fuse instead of boot configuration pins. If BT_FUSE_SEL=0, boot flow will jump to Serial Downloader.

0 Kudos