Hello Everyone,
I am working on porting BSP for IMX7 solo based custom board. When I looked in the DTS files, I can only see files related to IMX7 dual. For instance, all the name of dts files available for IMX7 starts with "imx7d_*.dts". Can you please say, where can I get the dts files for IMX7 solo? What are all the changes (in terms of building the source code and booting ) needed for IMX7 Solo?
解決済! 解決策の投稿を見る。
Hi Igor,
In WaRP7 board, they have used 12 X 12 Package of IMX7 solo. In our custom board we are planning to use 19 x 19 package of IMX7 solo (MCIMX7S5EVM08SC). So my doubt is, is it okay to use/refer WaRP7 board DTS file?
Hi Gopinath
one can look at Warp7 board which uses Solo :
linux-fslc/arch/arm/boot/dts at 4.1-1.0.x-imx · WaRP7/linux-fslc · GitHub
GitHub - WaRP7/WaRP7-User-Guide: WaRP7 User Guide Source. For binary releases go to the release tab
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
In WaRP7 board, they have used 12 X 12 Package of IMX7 solo. In our custom board we are planning to use 19 x 19 package of IMX7 solo (MCIMX7S5EVM08SC). So my doubt is, is it okay to use/refer WaRP7 board DTS file?
Hi Gopinath
yes okay, as processor is the same.
Best regards
igor
Thank You.