IMX7-Dual Boundary-scan on DDR pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7-Dual Boundary-scan on DDR pins

1,192 Views
ians1
Contributor I

Hello

We have one of your sabre development boards with the IMX7 dual processor populated. We are using it to prove the bsdl model supplied prior to a mutual customers production run.

Some of the IO pins follow the BSDL and can be toggled when the device is in boundary-scan/extest mode.

However none of the DDR pins (Address/data/control) toggle - they sit at 0.5V during test.

Is there any configuration (board or chip) required to turn on the ddr bank so the IMX7's "DDR" address/data and control pins toggle in extest?

(eg, IMX6 did have a register which needed programming to turn the EIM bus from highz drive value).

Thanks

Ian

Labels (1)
0 Kudos
Reply
1 Reply

1,119 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ian

I am afraid ddr testing with bsdl is not supported, some customers tried but

there were no known successful results.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply