(IMX6ulevk) Murata 1DX Module problem with broadcast and Interrupt from module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

(IMX6ulevk) Murata 1DX Module problem with broadcast and Interrupt from module

968件の閲覧回数
sebastianpszczo
Contributor I

Good Morning,

 

1. Connected murata 1DX module to IMX 6UltraLite EVK  using :  Murata uSD-M.2. Adapter + Embedded Artists M.2 Module.

2. Used Linux kernel supported by murata GitHub - murata-wireless/meta-murata-wireless  (branch imx-sumo-manda)

3. Connected to our AP without any problem and obtained IP address.

Prob

 

Problems started while receiving broadcast packets. We noticed that the 1DX module does not receive the vast majority of broadcast packages (about 60%). We can see on the oscilloscope that the 1DX module itself does not report OOB interrupts from incoming broadast packets. We did another test which showed that if we run the ping program in the background with a time of e.g. 100 milliseconds, the situation is better.

How can we solve this problem?

タグ(3)
0 件の賞賛
返信
1 返信

910件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bb Bbb,

This module is manufactured and supported by Murata. I would recommend contacting them for support as they may be better able to provide assistance.

Regards,

0 件の賞賛
返信