IMX6sx failed to boot from S25FL064L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6sx failed to boot from S25FL064L

1,997 Views
imx_proc_user
Contributor I

 

I have an issue with imx6sx boting with S25FL064L (use quad io). 

0a1804eb # lut[0] command sequence
0e081200 # lut[1] command sequence
24001e04 # lut[2] command sequence

Verified the norflash chip registers are as expected

read control register 1: 0x02
read control register 2: 0x00
read control register 3: 0x78
read status register 1: 0x02

After power cycle,  I have a BE/LE issue.  

I have boards, left is a board with S25FL132K, which is working properly; right side is the same board just replaced S25FL132K with S25FL064L.  Same u-boot is loaded.

jimzhang_0-1614104045778.jpeg

The QSPI is not configured properly, the ENG_CFG should be 0 if configured properly

The lut vlaue is loaded properly

If I manually load u-boot-spl and u-boot, they both work fine.

The problem is bootrom does not load the u-boot to ram, and not execute it.

Not sure what is broken in the boot sequence. Any suggestion is apprecaited.

Thanks,

Jim

 

 

0 Kudos
9 Replies

1,989 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jim

 

reason may be is that qspi configuration parameters were not updated for new qspi-nor,

described in Table 8-26. QuadSPI configuration parameters

i.MX 6SoloX Applications Processor Reference Manual

One can try to reprogram it using for example mfg tool (script mfgtool2-yocto-mx-sabresd-qspi-nor-n25q256a.vbs, samples:  qspi-nor-macronix-mx25l51245g-config, qspi-nor-micron-n25q256a-config

in folder ./files) , prepare new config file for S25FL064L

or with new uuu tool:  https://github.com/NXPmicro/mfgtools

sample script example_spinor.uuu can be found in Demo Images

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos

1,982 Views
imx_proc_user
Contributor I

Igor:

Thank you very much for the reply!

I have sample config for S25FL132K, and it is working on the old board. I used all those samples and figured out a new config. I uploaded it here with datasheet

Control Register 1: (Quad IO mode is enabled properly)

Control reister 2: (3-byte register mode is set)

Control register 3:  (dummy cycle is 8 cycles)

Status Register 1:  (write enable latch is set)

These are the right setting I need from the device.

The SEQID0 command to setup QSPI, which matches the s25fl064l datasheet:

0a1804eb

enable quad io read, 3 bytes address will be sent in 4 pads

0e081200

dummy cycle is 8 cycles, and mode uses 1 pad

24001e04

Read 4 bytes

 

The only instruction i am not sure is 1200. I was thinking it should be 0x1202: setting mode cycle to 2; but example tells set the number of pad for mode 

0 Kudos

1,976 Views
igorpadykov
NXP Employee
NXP Employee

so can you confirm that you flashed qspi-nor with modified qspi-nor-spansion-s25fl064l-config.txt

using mfg tool?

One can write them manually from uboot, for example load them to 0x80800000, then

write to qspi-nor from 0x400 offset:

sf write 0x80800000 0x400 0x200

 

0 Kudos

1,923 Views
imx_proc_user
Contributor I
I flashed the norchip with the configuration.  After power cycle, I manually loaded u-boot-spl to initialize the RAM, then I manually load u-boot to ram, and execute it. U-boot is able to run properly, norchip is detected by u-boot, and the config file can be read back from u-boot. Below is the output:
 
U-Boot 2015.07-g2e0d69a-dirty (Feb 19 2021 - 08:16:12 -0600)
CPU:   Freescale i.MX6SX rev1.3 at 792MHz
Reset cause: POR
Board: xxx
I2C:   ready
DRAM:  512 MiB
WARNING: Caches not enabled
PMIC:  PFUZE100 ID=0x11
MMC:   FSL_SDHC: 0
*** Warning - bad CRC, using default environment
In:    serial
Out:   serial
Err:   serial
Net:  FEC0 [PRIME]
Hit any key to stop autoboot:  0
=> sf probe
SF: Got idcodes
00000000: 01 60 17 ff                                        .`..
SF: Detected S25FL064L with page size 256 Bytes, erase size 64 KiB, total 8 MiB
=> sf read 0x80800000 0x400 0x400
device 0 offset 0x400, size 0x400
SF: 1024 bytes @ 0x400 Read: OK

=> md 0x80800000
80800000: 00000000 00000000 00000000 00000000    ................
80800010: 00000001 00000202 03000003 02000000    ................
80800020: 00000003 00000003 00800000 00000000    ................
80800030: 00000000 00000000 00000001 00000000    ................
80800040: 00000004 00000000 00000000 00000000    ................
80800050: 00000000 00000000 00000000 00000000    ................
80800060: 00000000 00000000 0a1804eb 0e081200    
80800070: 24001e04 00000000 1c010405 00002400    
80800080: 00000000 00000000 24000406 00000000    ........
80800090: 00000000 00000000 20010401 00002400    .......
808000a0: 00000000 00000000 00000000 00000000    ................
808000b0: 00000000 00000000 00000000 00000000    ................
808000c0: 00000000 00000000 00000000 00000000    ................
808000d0: 00000000 00000000 00000000 00000000    ................
808000e0: 00000000 00000000 00000000 00000000   
808000f0: 00000000 00000000 00000000 00000000
 
Manually execution seemed to be OK, but the board does not boot itself after power cycle
0 Kudos

1,907 Views
igorpadykov
NXP Employee
NXP Employee

one can try with image generated for S25FL132K, seems it is the same except nor size.

 

Best regards
igor

0 Kudos

1,900 Views
imx_proc_user
Contributor I

igor:

If the norflash content can be viewed correctly from qspi mapped address 0x60000000, it means the qspi configuration is correct, right?

How would bootrom interact with norchip ?  In what mode (single/dual/quad) it copies qspi configuration from 0x400 of the norchip? How does bootrom know what mode the chip is set ?

Thanks

Jim

 

0 Kudos

1,897 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jim

 

in general one can check non-volatile registers described on p.35

S25FL064L_64-Mbit_8-Mbyte_3.0_V_FL-L_SPI_Flash_Mem-1102570.pdf,

like QPI, Address Length at Power-up, e.t.c.

 

Best regards
igor

0 Kudos

1,885 Views
imx_proc_user
Contributor I

Those info is provided in the initial post. After power cycle, the non volatile registers are as fellows:

read control register 1:  0x02 (quad mode)
read control register 2:  0x00 (3-byte address)
read control register 3:  0x78 (8 dummy cycle)
read status register 1:  0x02  (write latch enabled)

0 Kudos

1,902 Views
imx_proc_user
Contributor I

Flashed working image for S25FL132k to the new board, and it failed the exact same way:

1: QSPI MCR has wrong endiness 

2: Reading norflash config/content from qspi mapped address 0x60001710, norflash content is correct.

Board still does not boot up itself.

0 Kudos