Dear All,
We are about to start a new satellite communication project and interested in the IMX6Ultra Lite EVK. I have downloaded i.MX 6UltraLite EVK - Quick Start Guide and reading through it. Also I am browsing i.MX 6 Series Software and Development Tool Resources page for downloading Linux BSP, documents and relevant SDK tools. However, I realized that non of the Linux BSP stating supporting for the IMX6Ultra Lite Evk. Also, in the quick start guide, Page11, "Download BSP Images" section, the firmwares (ie, u-boot-imx6ulevk_sd.imx) are not included in any of the package for Linux 3.14.28?
is Linux BSP for IMX6Ultra Lite Evk supported? Where can I find all the Linux BSP and SDK tools for IMX6Ultra lite Evk?
Thanks in advance.
已解决! 转到解答。
Hi Jimmy, Thanks for reply. Yes, the SDK are actually in the "Download" tab of i.MX6ULtraLite Evaluation Kit|NXP .
I have a related question:
We are working with the iMx6sx/sl processors, testing on the imx6-UltraLite and imx6-Sabre-Solo Boards.
I have been compiling the Images under Yocto on.
But, I can not find the relevant DTS files:
~/yocto_3.14.38-6UL/build/tmp/work/cortexa7hf-vfp-neon-poky-linux-gnueabi/linux-libc-headers/3.14-r0/linux-3.14/arch/arm/boot/dts $
imx6sl-evk.dts
imx6sl-pinfunc.h
imx6sl-warp.dts
imx6sl.dtsi
imx6sx-pinfunc.h
imx6sx-sabreauto.dts
imx6sx-sdb-reva.dts
imx6sx-sdb.dts
imx6sx-sdb.dtsi
imx6sx.dtsi
Why are these files missing (but I can still compile the Images for the Board),
and how do I add them to the Yocto source ?
... I need to add GPIO access in the DTS via the DTS files.