Hi!
I am designing imx6ull based board.
Not sure how to be with LCD_DATA pins that not used in my design at all.
Looking here:
https://www.nxp.com/docs/en/data-sheet/IMX6ULLCEC.pdf
I see table 78 " Fuses and Associated Pins Used for Boot" that says that
LCD_DATA00 - LCD_DATA23 pins reflects as input with 100k inputs pull-down
resistor.
I need only two of them to be pulled up during power up for boot configuration.
So, can I leave all other pins left floating at all if I need them only on boot configuration
process and I don't want to use external pull down resistors to save pcb space?