IMX6ULL processor TSC interface related Query?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL processor TSC interface related Query?

2,695 Views
ramesh6663
Contributor III

Hi,

In Imx6ull processor has internal 4/5 wire Resistive Touchscreen Controller so we don't require to use External TSC part through I2C/SPI communication as per my understanding.

Following are the signals used for TSC of LCD module. could you please provide the expansion of ynlr,ypll,xnur, xpul pin names.

I check with the reference design NXP EVK, I have doubt on the xnur, xpul signal connection. Please clarify us

As per my understanding :

xnur - X negative upper right side
xpul - X positive upper left side

ynlr - Y negative lower right side

ypll - Y positive lower left side

Is it correct?

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

2,372 Views
ramesh6663
Contributor III

Thanks Igor

0 Kudos
Reply

2,373 Views
igorpadykov
NXP Employee
NXP Employee

Hi ramesh

I think it is correct, unfortunately I am not aware of additional TSC documentation.

May be useful to check lcd datasheet which is used with i.MX6UL EVK board

Detail datasheet of LCD8000-43T 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,373 Views
ramesh6663
Contributor III

So I hope it will work directly to LCD which has those 4 signals. Am i right?

Or shall we need to add any buffer circuit inbetwenn SOC and LCD for touch screen signals?

0 Kudos
Reply

2,373 Views
igorpadykov
NXP Employee
NXP Employee

>it will work directly to LCD which has those 4 signals. Am i right?

right

Best regards
igor

0 Kudos
Reply