Hi Fabio
data loss is expected, as described in sect.55.8.2 UART Operation in System Stop Mode
i.MX 6ULL Applications Processor Reference Manual
"When an asynchronous WAKE (awake) interrupt exits the Arm platform from STOP
mode, make sure that a dummy character is sent first because the first character may not
be received correctly."
>Is it possible to configure the processor automatically goes in a low power mode when
>where is nothing to do?
it is already implemented in linux, one can check sect.2.5.1 Low Level Power Management (PM)
Linux Manual included in Linux L4.14.98_2.0.0 Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------