IMX6ULL - burn OCOTP block

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6ULL - burn OCOTP block

1,604 次查看
bbilas
Contributor I

Hello everyone,

I'm struggling with burning data into OCOTP block on IMX6ULL (MCIMX6Y2DVM05AB revision) using mainline U-Boot 2019.04. According to the reference manual, I try to write data into Bank7 Word0 using built-in fuse_prog function but I always get  `mxc_ocotp fuse_prog(): Access protect error` error despite the fact that the address, operation and value are valid. For the test purpose I've switched to the IMX6UL and I was there able to write data into OCOTP without any problem using the same code, changing only the bank. So my question is: is it possible to burn OCOTP block in IMX6ULL and if so, how to do that correctly?

Best

Bartek

标签 (1)
0 项奖励
回复
1 回复

1,498 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

I suggest you see the following document. Probably it can be useful to you.

https://community.nxp.com/docs/DOC-332776 

Best regards,

Diego.

0 项奖励
回复