IMX6ULL boot mode fuses via J-Link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL boot mode fuses via J-Link

543 Views
almaz1c
Contributor III

Hi!

Have custom pcb based on IMX6ULL.

Currently it boots using GPIO setup:

BOOT_MODE0 = 0, BOOT_MODE1 = 1,

BOOT_CFG1[3:0] = 0

BOOT_CFG1[7:4] = 0011 - Serial SPI

BOOT_CFG1[7:0] = 0

BOOT_CFG4[2:0] = 010 - ECSPI3

BOOT_CFG4[3] = 1 - SPI addressing 3 bytes. 

BOOT_CFG4[5:4] = 00 - CS - SS0 selected

BOOT_CFG4[6] = 0 - Disabled EEPROM recovery

We need to set booting interface using J-link for mass production. Able to connect to pcb using JTAG and detect MCU. Not sure how to burn fuse modes according to configuration above. Does anyone has experience with it?

Labels (1)
0 Kudos
1 Reply

498 Views
igorpadykov
NXP Employee
NXP Employee

Hi Almaz

nxp does not support fuse programming with jtag, in general one can write

script reusing programming commands from baremetal sdk

rt-thread/bsp/imx6sx/iMX6_Platform_SDK/sdk/drivers/ocotp at master · RT-Thread/rt-thread · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos