IMX6ULL - TFT 240x320 display - ili9341 driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6ULL - TFT 240x320 display - ili9341 driver

3,737 次查看
dudisasson
Contributor I

Hi,

i am trying to connect a TFT display with ili9341 driver to a imx6ull som. the default display for this som is a 800x600 touchscreen.

i want to work with the display in RGB666 mode.

I was able to get the display to work with the following setup:

-The lcd data and control lines and are connected to the som.

-The SPI lines are connected to a small MCU that configures the display.

Now i want to configure the display using the SOM. I`ve connected the SPI lines to ECSPI1. I also connected the DC and Reset pins.

I`ve added the driver from the following patch and enabled it using the menuconfig.

[RFC,1/2] drm/panel: Add Ilitek ILI9341 parallel RGB panel driver - Patchwork 

This is the configuration i am using in the device tree:

&lcdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcdif_dat
&pinctrl_lcdif_ctrl>;
display = <&display0>;
backlight = <&backlight_0>;
status = "okay";

display0: display {
bits-per-pixel = <16>;
bus-width = <18>;

display-timings {
native-mode = <&timing0>;
timing0: timing0 {
clock-frequency = <6350000>;
hactive = <240>;
vactive = <320>;
hfront-porch = <10>;
hback-porch = <20>;
hsync-len = <10>;
vback-porch = <2>;
vfront-porch = <4>;
vsync-len = <2>;

hsync-active = <0>;
vsync-active = <0>;
de-active = <1>;
pixelclk-active = <0>;
};
};

port@0 {
display_out: endpoint {
remote-endpoint = <&panel_in>;
};
};
};



};

&ecspi1 {
fsl,spi-num-chipselects = <1>;
cs-gpios = <&gpio3 26 0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi1>;
status = "okay";

panel@0 {
compatible = "displaytech,dt024ctft", "ilitek,ili9341";
reg = <0>;
spi-max-frequency = <32000000>;
dc-gpios = <&gpio1 8 GPIO_ACTIVE_HIGH>;
//reset-gpios = <&gpio3 4 GPIO_ACTIVE_LOW>;
backlight = <&backlight_0>;

port {
panel_in: endpoint {
remote-endpoint = <&display_out>;
};
};

};
};

The SPI is registered:

root@visionsom:/dev# dmesg | grep spi0

[    1.677264] spi_imx 2008000.spi: registered master spi0

[    1.677648] spi spi0.0: spi_imx_setup: mode 0, 8 bpw, 32000000 hz

[    1.677690] spi spi0.0: setup mode 0, 8 bits/w, 32000000 Hz max --> 0

[    1.678181] spi_imx 2008000.spi: registered child spi0.0

and the display is configured in the right resolution:

root@visionsom:~# fbset

 

mode "240x320-69"

    # D: 6.350 MHz, H: 22.679 kHz, V: 69.142 Hz

    geometry 240 320 240 320 16

    timings 157480 20 10 2 4 10 2

    sync 0x40000000

    rgba 5/11,6/5,5/0,0/0

endmode

but i am not seeing any data in the spi lines.

do i need to add anything else to enable the driver?

do i need to do something from the userspace/Uboot?

Thanks,

Dudi.

标签 (2)
0 项奖励
回复
3 回复数

3,624 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dudi

for lcds with ecspi one can look at examples:

How to use SPI slave within U-Boot? 

https://community.nxp.com/thread/451152 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,624 次查看
dudisasson
Contributor I

Hi Igor,

Thank you for the quick repsonse.

i just want to clarify that i want to use the parallel mode of the display.

i was able to link the spi to the ili9341 driver and now i am getting the following:

root@visionsom:~# dmesg | grep spi0

[ 1.469158] spi_imx 2008000.spi: registered master spi0

[ 1.469557] spi spi0.0: spi_imx_setup: mode 0, 8 bpw, 32000000 hz

[ 1.469597] spi spi0.0: setup mode 0, 8 bits/w, 32000000 Hz max --> 0

[ 1.470313] panel-ilitek-ili9341 spi0.0: spi_imx_setup: mode 0, 8 bpw, 32000000 hz

[ 1.470351] panel-ilitek-ili9341 spi0.0: setup mode 0, 8 bits/w, 32000000 Hz max --> 0

[ 1.470468] spi_imx 2008000.spi: registered child spi0.0

it seems i need to enable the driver but i cant understand how.

0 项奖励
回复

3,624 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dudi

for parallel lcd first one can try to enable it in uboot,

refer to function do_enable_parallel_lcd() in:

mx6ullevk.c\mx6ullevk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor

0 项奖励
回复