IMX6ULL GPIO device tree customization

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6ULL GPIO device tree customization

2,656 次查看
vasudhevan
Contributor V

I referred many community links not fully understood.

I checked with sd card detect pin it's working fine.

  1. It's compulsory uboot device tree also needs to modify ? 
  2. Both uboot and kernel device tree should be same ?
  3. Can i get example kernel device tree structure for gpio and input button customization ?
  4. How this customization imx gpio device driver knows and how its working ?

Regards

Vasu

标签 (3)
0 项奖励
回复
1 回复

2,371 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vasu

it is not necessary to use uboot device tree and general overview for both can be found on web:

arm - Why Device Tree Structure (DTS) file is needed both in bootloader and kernel source code? - St... 

for gpio and device tree customization one can look on

https://boundarydevices.com/mx6-device-tree-customization/ 

Definitive GPIO guide - Studio Kousagi Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复