Hi,
I found a lot of topic with this argument but onestly I didn't understood ...
My problem is very easy apparently ... I have developed an application on IMX6ULL EVK and
now I have to port my application on the real board.
The first problem is the difference about the GPIO management.
How is possible to change this feature using the DTSI file?
How is possible to configure a GPIO adding some directive in the DTSI file?
For example ... in my IMX6ULL EVK I have
&tsc {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_tsc>;
xnur-gpio = <&gpio1 3 GPIO_ACTIVE_LOW>;
 measure-delay-time = <0xffff>;
 pre-charge-time = <0xfff>;
 status = "okay";
};
how is possible to use the xnur_gpio (MX6UL_PAD_GPIO1_IO03__GPIO1_IO03) as
GPIO configured as an output?
Thanks
Fabio
I'm not able to do that :-(
for example .. I need to set to 1 the GPIO4_IO20 ....
how can I do that?
this is my dts file ..
/*
 * Copyright (C) 2016 Freescale Semiconductor, Inc.
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License version 2 as
 * published by the Free Software Foundation.
 */
/dts-v1/;
#include <dt-bindings/input/input.h>
#include "imx6ull.dtsi"
/* my define set 1 */
#define MX6UL_PAD_CSI_HSYNC__GPIO4_IO20_1 0x01e0 0x046c 0x0000 5 1
/* my define */
/ {
 model = "Freescale i.MX6 ULL 14x14 EVK Board";
 compatible = "fsl,imx6ull-14x14-evk", "fsl,imx6ull";
chosen {
 stdout-path = &uart1;
 };
memory {
 reg = <0x80000000 0x20000000>;
 };
reserved-memory {
 #address-cells = <1>;
 #size-cells = <1>;
 ranges;
linux,cma {
 compatible = "shared-dma-pool";
 reusable;
 size = <0x14000000>;
 linux,cma-default;
 };
 };
backlight {
 compatible = "pwm-backlight";
 pwms = <&pwm1 0 5000000>;
 brightness-levels = <0 4 8 16 32 64 128 255>;
 default-brightness-level = <6>;
 status = "okay";
 };
pxp_v4l2 {
 compatible = "fsl,imx6ul-pxp-v4l2", "fsl,imx6sx-pxp-v4l2", "fsl,imx6sl-pxp-v4l2";
 status = "okay";
 };
regulators {
 compatible = "simple-bus";
 #address-cells = <1>;
 #size-cells = <0>;
reg_can_3v3: regulator@0 {
 compatible = "regulator-fixed";
 reg = <0>;
 regulator-name = "can-3v3";
 regulator-min-microvolt = <3300000>;
 regulator-max-microvolt = <3300000>;
 gpios = <&gpio_spi 3 GPIO_ACTIVE_LOW>;
 };
reg_sd1_vmmc: regulator@1 {
 compatible = "regulator-fixed";
 regulator-name = "VSD_3V3";
 regulator-min-microvolt = <3300000>;
 regulator-max-microvolt = <3300000>;
 gpio = <&gpio1 9 GPIO_ACTIVE_HIGH>;
 off-on-delay = <20000>;
 enable-active-high;
 };
reg_vref_adc: regulator-vref-adc {
 compatible = "regulator-fixed";
 regulator-name = "vref-adc";
 regulator-min-microvolt = <3300000>;
 regulator-max-microvolt = <3300000>;
 status = "okay";
 };
reg_gpio_dvfs: regulator-gpio {
 compatible = "regulator-gpio";
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_dvfs>;
 regulator-min-microvolt = <1300000>;
 regulator-max-microvolt = <1400000>;
 regulator-name = "gpio_dvfs";
 regulator-type = "voltage";
 gpios = <&gpio5 3 GPIO_ACTIVE_HIGH>;
 states = <1300000 0x1 1400000 0x0>;
 };
 };
sound {
 compatible = "fsl,imx6ul-evk-wm8960",
 "fsl,imx-audio-wm8960";
 model = "wm8960-audio";
 cpu-dai = <&sai2>;
// audio-codec = <&codec>;
 asrc-controller = <&asrc>;
 codec-master;
 gpr = <&gpr 4 0x100000 0x100000>;
 /*
 * hp-det = <hp-det-pin hp-det-polarity>;
 * hp-det-pin: JD1 JD2 or JD3
 * hp-det-polarity = 0: hp detect high for headphone
 * hp-det-polarity = 1: hp detect high for speaker
 */
 hp-det = <3 0>;
 hp-det-gpios = <&gpio5 4 0>;
 mic-det-gpios = <&gpio5 4 0>;
 audio-routing =
 "Headphone Jack", "HP_L",
 "Headphone Jack", "HP_R",
 "Ext Spk", "SPK_LP",
 "Ext Spk", "SPK_LN",
 "Ext Spk", "SPK_RP",
 "Ext Spk", "SPK_RN",
 "LINPUT2", "Mic Jack",
 "LINPUT3", "Mic Jack",
 "RINPUT1", "Main MIC",
 "RINPUT2", "Main MIC",
 "Mic Jack", "MICB",
 "Main MIC", "MICB",
 "CPU-Playback", "ASRC-Playback",
 "Playback", "CPU-Playback",
 "ASRC-Capture", "CPU-Capture",
 "CPU-Capture", "Capture";
 };
spi4 {
 compatible = "spi-gpio";
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_spi4>;
 pinctrl-assert-gpios = <&gpio5 8 GPIO_ACTIVE_LOW>;
 status = "okay";
 gpio-sck = <&gpio5 11 0>;
 gpio-mosi = <&gpio5 10 0>;
 cs-gpios = <&gpio5 7 0>;
 num-chipselects = <1>;
 #address-cells = <1>;
 #size-cells = <0>;
gpio_spi: gpio_spi@0 {
 compatible = "fairchild,74hc595";
 gpio-controller;
 #gpio-cells = <2>;
 reg = <0>;
 registers-number = <1>;
 registers-default = /bits/ 8 <0x57>;
 spi-max-frequency = <100000>;
 };
 };
};
&cpu0 {
 dc-supply = <®_gpio_dvfs>;
};
&clks {
 assigned-clocks = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
 assigned-clock-rates = <786432000>;
};
/*
&csi {
 status = "okay";
 port {
 csi1_ep: endpoint {
 remote-endpoint = <&ov5640_ep>;
 };
 };
};
*/
/* fabio sarebbe quella buona 
&fec1 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_enet1>;
 phy-mode = "rmii";
 phy-handle = <ðphy0>;
 status = "okay";
mdio {
 #address-cells = <1>;
 #size-cells = <0>;
ethphy0: ethernet-phy@0 {
 compatible = "ethernet-phy-ieee802.3-c22";
 reg = <1>;
 micrel,led-mode = <1>;
 clocks = <&clks IMX6UL_CLK_ENET_REF>;
 clock-names = "rmii-ref";
 };
};
};
*/
&fec1 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_enet1>;
 phy-mode = "rmii";
 phy-handle = <ðphy0>;
 status = "okay";
mdio {
 #address-cells = <1>;
 #size-cells = <0>;
ethphy0: ethernet-phy@0 {
 compatible = "ethernet-phy-ieee802.3-c22";
 reg = <1>;
 micrel,led-mode = <1>;
 clocks = <&clks IMX6UL_CLK_ENET_REF>;
 clock-names = "rmii-ref";
 };
};
};
&flexcan1 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_flexcan1>;
 xceiver-supply = <®_can_3v3>;
 status = "okay";
};
&flexcan2 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_flexcan2>;
 xceiver-supply = <®_can_3v3>;
 status = "okay";
};
&gpc {
 fsl,cpu_pupscr_sw2iso = <0xf>;
 fsl,cpu_pupscr_sw = <0x0>;
 fsl,cpu_pdnscr_iso2sw = <0x1>;
 fsl,cpu_pdnscr_iso = <0x1>;
 fsl,ldo-bypass = <0>; /* DCDC, ldo-enable */
};
/* &i2c1 {
 clock-frequency = <100000>;
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_i2c1>;
 status = "okay";
mag3110@0e {
 compatible = "fsl,mag3110";
 reg = <0x0e>;
 position = <2>;
 };
fxls8471@1e {
 compatible = "fsl,fxls8471";
 reg = <0x1e>;
 position = <0>;
 interrupt-parent = <&gpio5>;
 interrupts = <0 8>;
 };
};
*/
/* &i2c2 {
 clock_frequency = <100000>;
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_i2c2>;
 status = "okay";
codec: wm8960@1a {
 compatible = "wlf,wm8960";
 reg = <0x1a>;
 clocks = <&clks IMX6UL_CLK_SAI2>;
 clock-names = "mclk";
 wlf,shared-lrclk;
 };
ov5640: ov5640@3c {
 compatible = "ovti,ov5640";
 reg = <0x3c>;
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_csi1>;
 clocks = <&clks IMX6UL_CLK_CSI>;
 clock-names = "csi_mclk";
 pwn-gpios = <&gpio_spi 6 1>;
 rst-gpios = <&gpio_spi 5 0>;
 csi_id = <0>;
 mclk = <24000000>;
 mclk_source = <0>;
 status = "okay";
 port {
 ov5640_ep: endpoint {
 remote-endpoint = <&csi1_ep>;
 };
 };
 };
};
*/
&iomuxc {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_hog_1>;
 pinctrl_hog_1: hoggrp-1 {
 fsl,pins = <
 MX6UL_PAD_UART1_RTS_B__GPIO1_IO19 0x17059 /* SD1 CD */
// MX6UL_PAD_GPIO1_IO05__USDHC1_VSELECT 0x17059 /* SD1 VSELECT */
// MX6UL_PAD_GPIO1_IO09__GPIO1_IO09 0x17059 /* SD1 RESET */
 >;
 };
 pinctrl_csi1: csi1grp {
 fsl,pins = <
 MX6UL_PAD_CSI_MCLK__CSI_MCLK 0x1b088
 MX6UL_PAD_CSI_PIXCLK__CSI_PIXCLK 0x1b088
 MX6UL_PAD_CSI_VSYNC__GPIO4_IO19 0x1b088
// MX6UL_PAD_CSI_VSYNC__CSI_VSYNC 0x1b088
 MX6UL_PAD_CSI_HSYNC__GPIO4_IO20 0x1b088
// MX6UL_PAD_CSI_HSYNC__CSI_HSYNC 0x1b088
 MX6UL_PAD_CSI_DATA00__CSI_DATA02 0x1b088
 MX6UL_PAD_CSI_DATA01__CSI_DATA03 0x1b088
 MX6UL_PAD_CSI_DATA02__CSI_DATA04 0x1b088
 MX6UL_PAD_CSI_DATA03__CSI_DATA05 0x1b088
 MX6UL_PAD_CSI_DATA04__CSI_DATA06 0x1b088
 MX6UL_PAD_CSI_DATA05__CSI_DATA07 0x1b088
 MX6UL_PAD_CSI_DATA06__CSI_DATA08 0x1b088
 MX6UL_PAD_CSI_DATA07__CSI_DATA09 0x1b088
 >;
 };
pinctrl_enet1: enet1grp {
 fsl,pins = <
 MX6UL_PAD_ENET1_RX_EN__ENET1_RX_EN 0x1b0b0
 MX6UL_PAD_ENET1_RX_ER__ENET1_RX_ER 0x1b0b0
 MX6UL_PAD_ENET1_RX_DATA0__ENET1_RDATA00 0x1b0b0
 MX6UL_PAD_ENET1_RX_DATA1__ENET1_RDATA01 0x1b0b0
 MX6UL_PAD_ENET1_TX_EN__ENET1_TX_EN 0x1b0b0
 MX6UL_PAD_ENET1_TX_DATA0__ENET1_TDATA00 0x1b0b0
 MX6UL_PAD_ENET1_TX_DATA1__ENET1_TDATA01 0x1b0b0
 MX6UL_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x4001b031
/* fabio */
 // MX6UL_PAD_ENET2_RX_DATA0__ENET1_MDIO 0x1b0b0
 // MX6UL_PAD_ENET2_RX_DATA1__ENET1_MDC 0x1b0b0
 MX6UL_PAD_GPIO1_IO06__ENET1_MDIO 0x1b0b0
 MX6UL_PAD_GPIO1_IO07__ENET1_MDC 0x1b0b0
/* fabio */
 >;
 };
 pinctrl_flexcan1: flexcan1grp{
 fsl,pins = <
 MX6UL_PAD_UART3_RTS_B__FLEXCAN1_RX 0x1b020
 MX6UL_PAD_UART3_CTS_B__FLEXCAN1_TX 0x1b020
 >;
 };
pinctrl_flexcan2: flexcan2grp{
 fsl,pins = <
 MX6UL_PAD_UART2_RTS_B__FLEXCAN2_RX 0x1b020
 MX6UL_PAD_UART2_CTS_B__FLEXCAN2_TX 0x1b020
 >;
 };
pinctrl_i2c1: i2c1grp {
 fsl,pins = <
 MX6UL_PAD_UART4_TX_DATA__I2C1_SCL 0x4001b8b0
 MX6UL_PAD_UART4_RX_DATA__I2C1_SDA 0x4001b8b0
 >;
 };
/* pinctrl_i2c2: i2c2grp {
 fsl,pins = <
 MX6UL_PAD_UART5_TX_DATA__I2C2_SCL 0x4001b8b0
 MX6UL_PAD_UART5_RX_DATA__I2C2_SDA 0x4001b8b0
 >;
 };
*/
 pinctrl_lcdif_dat: lcdifdatgrp {
 fsl,pins = <
 MX6UL_PAD_LCD_DATA00__LCDIF_DATA00 0x79
 MX6UL_PAD_LCD_DATA01__LCDIF_DATA01 0x79
 MX6UL_PAD_LCD_DATA02__LCDIF_DATA02 0x79
 MX6UL_PAD_LCD_DATA03__LCDIF_DATA03 0x79
 MX6UL_PAD_LCD_DATA04__LCDIF_DATA04 0x79
 MX6UL_PAD_LCD_DATA05__LCDIF_DATA05 0x79
 MX6UL_PAD_LCD_DATA06__LCDIF_DATA06 0x79
 MX6UL_PAD_LCD_DATA07__LCDIF_DATA07 0x79
 MX6UL_PAD_LCD_DATA08__LCDIF_DATA08 0x79
 MX6UL_PAD_LCD_DATA09__LCDIF_DATA09 0x79
 MX6UL_PAD_LCD_DATA10__LCDIF_DATA10 0x79
 MX6UL_PAD_LCD_DATA11__LCDIF_DATA11 0x79
 MX6UL_PAD_LCD_DATA12__LCDIF_DATA12 0x79
 MX6UL_PAD_LCD_DATA13__LCDIF_DATA13 0x79
 MX6UL_PAD_LCD_DATA14__LCDIF_DATA14 0x79
 MX6UL_PAD_LCD_DATA15__LCDIF_DATA15 0x79
 MX6UL_PAD_LCD_DATA16__LCDIF_DATA16 0x79
 MX6UL_PAD_LCD_DATA17__LCDIF_DATA17 0x79
 MX6UL_PAD_LCD_DATA18__LCDIF_DATA18 0x79
 MX6UL_PAD_LCD_DATA19__LCDIF_DATA19 0x79
 MX6UL_PAD_LCD_DATA20__LCDIF_DATA20 0x79
 MX6UL_PAD_LCD_DATA21__LCDIF_DATA21 0x79
 MX6UL_PAD_LCD_DATA22__LCDIF_DATA22 0x79
 MX6UL_PAD_LCD_DATA23__LCDIF_DATA23 0x79
 >;
 };
pinctrl_lcdif_ctrl: lcdifctrlgrp {
 fsl,pins = <
 MX6UL_PAD_LCD_CLK__LCDIF_CLK 0x79
 MX6UL_PAD_LCD_ENABLE__LCDIF_ENABLE 0x79
 MX6UL_PAD_LCD_HSYNC__LCDIF_HSYNC 0x79
 MX6UL_PAD_LCD_VSYNC__LCDIF_VSYNC 0x79
 >;
 };
pinctrl_pwm1: pwm1grp {
 fsl,pins = <
// MX6UL_PAD_GPIO1_IO08__PWM1_OUT 0x110b0
 >;
 };
pinctrl_qspi: qspigrp {
 fsl,pins = <
 MX6UL_PAD_NAND_WP_B__QSPI_A_SCLK 0x70a1
 MX6UL_PAD_NAND_READY_B__QSPI_A_DATA00 0x70a1
 MX6UL_PAD_NAND_CE0_B__QSPI_A_DATA01 0x70a1
 MX6UL_PAD_NAND_CE1_B__QSPI_A_DATA02 0x70a1
 MX6UL_PAD_NAND_CLE__QSPI_A_DATA03 0x70a1
 MX6UL_PAD_NAND_DQS__QSPI_A_SS0_B 0x70a1
 >;
 };
pinctrl_sai2: sai2grp {
 fsl,pins = <
 MX6UL_PAD_JTAG_TDI__SAI2_TX_BCLK 0x17088
 MX6UL_PAD_JTAG_TDO__SAI2_TX_SYNC 0x17088
 MX6UL_PAD_JTAG_TRST_B__SAI2_TX_DATA 0x11088
 MX6UL_PAD_JTAG_TCK__SAI2_RX_DATA 0x11088
 MX6UL_PAD_JTAG_TMS__SAI2_MCLK 0x17088
 >;
 };
/* fabio pinctrl_tsc: tscgrp {
 fsl,pins = <
 MX6UL_PAD_GPIO1_IO01__GPIO1_IO01 0xb0
 MX6UL_PAD_GPIO1_IO02__GPIO1_IO02 0xb0
 MX6UL_PAD_GPIO1_IO03__GPIO1_IO03 0xb0
 MX6UL_PAD_GPIO1_IO04__GPIO1_IO04 0xb0
 >;
 };
*/
 pinctrl_uart1: uart1grp {
 fsl,pins = <
 MX6UL_PAD_UART1_TX_DATA__UART1_DCE_TX 0x1b0b1
 MX6UL_PAD_UART1_RX_DATA__UART1_DCE_RX 0x1b0b1
 >;
 };
pinctrl_uart2: uart2grp {
 fsl,pins = <
 MX6UL_PAD_UART2_TX_DATA__UART2_DCE_TX 0x1b0b1
 MX6UL_PAD_UART2_RX_DATA__UART2_DCE_RX 0x1b0b1
 MX6UL_PAD_UART3_RX_DATA__UART2_DCE_RTS 0x1b0b1
 MX6UL_PAD_UART3_TX_DATA__UART2_DCE_CTS 0x1b0b1
 >;
 };
pinctrl_uart2dte: uart2dtegrp {
 fsl,pins = <
 MX6UL_PAD_UART2_TX_DATA__UART2_DTE_RX 0x1b0b1
 MX6UL_PAD_UART2_RX_DATA__UART2_DTE_TX 0x1b0b1
 MX6UL_PAD_UART3_RX_DATA__UART2_DTE_CTS 0x1b0b1
 MX6UL_PAD_UART3_TX_DATA__UART2_DTE_RTS 0x1b0b1
 >;
 };
/* fabio */
 pinctrl_uart4: uart4grp {
 fsl,pins = <
 MX6UL_PAD_UART4_TX_DATA__UART4_DCE_TX 0x1b0b1
 MX6UL_PAD_UART4_RX_DATA__UART4_DCE_RX 0x1b0b1
 >;
 };
pinctrl_uart5: uart5grp {
 fsl,pins = <
 MX6UL_PAD_UART5_TX_DATA__UART5_DCE_TX 0x1b0b1
 MX6UL_PAD_UART5_RX_DATA__UART5_DCE_RX 0x1b0b1
 >;
 };
/* fabio */
pinctrl_usb_otg1_id: usbotg1idgrp {
 fsl,pins = <
// MX6UL_PAD_GPIO1_IO00__ANATOP_OTG1_ID 0x17059
 >;
 };
pinctrl_usdhc1: usdhc1grp {
 fsl,pins = <
 MX6UL_PAD_SD1_CMD__USDHC1_CMD 0x17059
 MX6UL_PAD_SD1_CLK__USDHC1_CLK 0x10071
 MX6UL_PAD_SD1_DATA0__USDHC1_DATA0 0x17059
 MX6UL_PAD_SD1_DATA1__USDHC1_DATA1 0x17059
 MX6UL_PAD_SD1_DATA2__USDHC1_DATA2 0x17059
 MX6UL_PAD_SD1_DATA3__USDHC1_DATA3 0x17059
 >;
 };
pinctrl_usdhc1_100mhz: usdhc1grp100mhz {
 fsl,pins = <
 MX6UL_PAD_SD1_CMD__USDHC1_CMD 0x170b9
 MX6UL_PAD_SD1_CLK__USDHC1_CLK 0x100b9
 MX6UL_PAD_SD1_DATA0__USDHC1_DATA0 0x170b9
 MX6UL_PAD_SD1_DATA1__USDHC1_DATA1 0x170b9
 MX6UL_PAD_SD1_DATA2__USDHC1_DATA2 0x170b9
 MX6UL_PAD_SD1_DATA3__USDHC1_DATA3 0x170b9
 >;
 };
pinctrl_usdhc1_200mhz: usdhc1grp200mhz {
 fsl,pins = <
 MX6UL_PAD_SD1_CMD__USDHC1_CMD 0x170f9
 MX6UL_PAD_SD1_CLK__USDHC1_CLK 0x100f9
 MX6UL_PAD_SD1_DATA0__USDHC1_DATA0 0x170f9
 MX6UL_PAD_SD1_DATA1__USDHC1_DATA1 0x170f9
 MX6UL_PAD_SD1_DATA2__USDHC1_DATA2 0x170f9
 MX6UL_PAD_SD1_DATA3__USDHC1_DATA3 0x170f9
 >;
 };
pinctrl_usdhc2: usdhc2grp {
 fsl,pins = <
 MX6UL_PAD_NAND_RE_B__USDHC2_CLK 0x10069
 MX6UL_PAD_NAND_WE_B__USDHC2_CMD 0x17059
 MX6UL_PAD_NAND_DATA00__USDHC2_DATA0 0x17059
 MX6UL_PAD_NAND_DATA01__USDHC2_DATA1 0x17059
 MX6UL_PAD_NAND_DATA02__USDHC2_DATA2 0x17059
 MX6UL_PAD_NAND_DATA03__USDHC2_DATA3 0x17059
 >;
 };
 pinctrl_usdhc2_8bit: usdhc2grp_8bit {
 fsl,pins = <
 MX6UL_PAD_NAND_RE_B__USDHC2_CLK 0x10069
 MX6UL_PAD_NAND_WE_B__USDHC2_CMD 0x17059
 MX6UL_PAD_NAND_DATA00__USDHC2_DATA0 0x17059
 MX6UL_PAD_NAND_DATA01__USDHC2_DATA1 0x17059
 MX6UL_PAD_NAND_DATA02__USDHC2_DATA2 0x17059
 MX6UL_PAD_NAND_DATA03__USDHC2_DATA3 0x17059
 MX6UL_PAD_NAND_DATA04__USDHC2_DATA4 0x17059
 MX6UL_PAD_NAND_DATA05__USDHC2_DATA5 0x17059
 MX6UL_PAD_NAND_DATA06__USDHC2_DATA6 0x17059
 MX6UL_PAD_NAND_DATA07__USDHC2_DATA7 0x17059
 >;
 };
 pinctrl_usdhc2_8bit_100mhz: usdhc2grp_8bit_100mhz {
 fsl,pins = <
 MX6UL_PAD_NAND_RE_B__USDHC2_CLK 0x100b9
 MX6UL_PAD_NAND_WE_B__USDHC2_CMD 0x170b9
 MX6UL_PAD_NAND_DATA00__USDHC2_DATA0 0x170b9
 MX6UL_PAD_NAND_DATA01__USDHC2_DATA1 0x170b9
 MX6UL_PAD_NAND_DATA02__USDHC2_DATA2 0x170b9
 MX6UL_PAD_NAND_DATA03__USDHC2_DATA3 0x170b9
 MX6UL_PAD_NAND_DATA04__USDHC2_DATA4 0x170b9
 MX6UL_PAD_NAND_DATA05__USDHC2_DATA5 0x170b9
 MX6UL_PAD_NAND_DATA06__USDHC2_DATA6 0x170b9
 MX6UL_PAD_NAND_DATA07__USDHC2_DATA7 0x170b9
 >;
 };
pinctrl_usdhc2_8bit_200mhz: usdhc2grp_8bit_200mhz {
 fsl,pins = <
 MX6UL_PAD_NAND_RE_B__USDHC2_CLK 0x100f9
 MX6UL_PAD_NAND_WE_B__USDHC2_CMD 0x170f9
 MX6UL_PAD_NAND_DATA00__USDHC2_DATA0 0x170f9
 MX6UL_PAD_NAND_DATA01__USDHC2_DATA1 0x170f9
 MX6UL_PAD_NAND_DATA02__USDHC2_DATA2 0x170f9
 MX6UL_PAD_NAND_DATA03__USDHC2_DATA3 0x170f9
 MX6UL_PAD_NAND_DATA04__USDHC2_DATA4 0x170f9
 MX6UL_PAD_NAND_DATA05__USDHC2_DATA5 0x170f9
 MX6UL_PAD_NAND_DATA06__USDHC2_DATA6 0x170f9
 MX6UL_PAD_NAND_DATA07__USDHC2_DATA7 0x170f9
 >;
 };
 pinctrl_wdog: wdoggrp {
 fsl,pins = <
 MX6UL_PAD_LCD_RESET__WDOG1_WDOG_ANY 0x30b0
 >;
 };
pinctrl_adc1: adc1grp {
 fsl,pins = <
 MX6UL_PAD_GPIO1_IO00__GPIO1_IO00 0x010b0
 MX6UL_PAD_GPIO1_IO01__GPIO1_IO01 0x010b0
 MX6UL_PAD_GPIO1_IO02__GPIO1_IO02 0x010b0
 MX6UL_PAD_GPIO1_IO03__GPIO1_IO03 0x010b0
 MX6UL_PAD_GPIO1_IO04__GPIO1_IO04 0x010b0
 MX6UL_PAD_GPIO1_IO05__GPIO1_IO05 0x010b0
 MX6UL_PAD_GPIO1_IO08__GPIO1_IO08 0x010b0
 MX6UL_PAD_GPIO1_IO09__GPIO1_IO09 0x010b0
 >;
 };
};
&iomuxc_snvs {
 pinctrl-names = "default_snvs";
 pinctrl-0 = <&pinctrl_hog_2>;
 imx6ul-evk {
 pinctrl_hog_2: hoggrp-2 {
 fsl,pins = <
 MX6ULL_PAD_SNVS_TAMPER0__GPIO5_IO00 0x80000000
 >;
 };
pinctrl_dvfs: dvfsgrp {
 fsl,pins = <
 MX6ULL_PAD_SNVS_TAMPER3__GPIO5_IO03 0x79
 >;
 };
 
 pinctrl_lcdif_reset: lcdifresetgrp {
 fsl,pins = <
 /* used for lcd reset */
 MX6ULL_PAD_SNVS_TAMPER9__GPIO5_IO09 0x79
 >;
 };
pinctrl_spi4: spi4grp {
 fsl,pins = <
 MX6ULL_PAD_BOOT_MODE0__GPIO5_IO10 0x70a1
 MX6ULL_PAD_BOOT_MODE1__GPIO5_IO11 0x70a1
 MX6ULL_PAD_SNVS_TAMPER7__GPIO5_IO07 0x70a1
 MX6ULL_PAD_SNVS_TAMPER8__GPIO5_IO08 0x80000000
 >;
 };
pinctrl_sai2_hp_det_b: sai2_hp_det_grp {
 fsl,pins = <
 MX6ULL_PAD_SNVS_TAMPER4__GPIO5_IO04 0x17059
 >;
 };
 };
};
&lcdif {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_lcdif_dat
 &pinctrl_lcdif_ctrl
 &pinctrl_lcdif_reset>;
 display = <&display0>;
 status = "okay";
display0: display@0 {
 bits-per-pixel = <16>;
 bus-width = <24>;
display-timings {
 native-mode = <&timing0>;
 timing0: timing0 {
 clock-frequency = <9200000>;
 hactive = <480>;
 vactive = <272>;
 hfront-porch = <8>;
 hback-porch = <4>;
 hsync-len = <41>;
 vback-porch = <2>;
 vfront-porch = <4>;
 vsync-len = <10>;
hsync-active = <0>;
 vsync-active = <0>;
 de-active = <1>;
 pixelclk-active = <0>;
 };
 };
 };
};
&pwm1 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_pwm1>;
 status = "okay";
};
&pxp {
 status = "okay";
};
&qspi {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_qspi>;
 status = "okay";
 ddrsmp=<0>;
flash0: n25q256a@0 {
 #address-cells = <1>;
 #size-cells = <1>;
 compatible = "micron,n25q256a";
 spi-max-frequency = <29000000>;
 spi-nor,ddr-quad-read-dummy = <6>;
 reg = <0>;
 };
};
&sai2 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_sai2
 &pinctrl_sai2_hp_det_b>;
assigned-clocks = <&clks IMX6UL_CLK_SAI2_SEL>,
 <&clks IMX6UL_CLK_SAI2>;
 assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
 assigned-clock-rates = <0>, <12288000>;
status = "okay";
};
/* &tsc {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_tsc>;
 xnur-gpio = <&gpio1 3 GPIO_ACTIVE_LOW>;
 measure-delay-time = <0xffff>;
 pre-charge-time = <0xfff>;
 status = "okay";
};
*/
&uart1 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_uart1>;
 status = "okay";
};
&uart2 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_uart2>;
 fsl,uart-has-rtscts;
 /* for DTE mode, add below change */
 /* fsl,dte-mode; */
 /* pinctrl-0 = <&pinctrl_uart2dte>; */
 status = "okay";
};
/* fabio */
&uart4 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_uart4>;
 fsl,uart-has-rtscts;
 status = "okay";
};
&uart5 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_uart5>;
 fsl,uart-has-rtscts;
 status = "okay";
};
/* fabio */
/* fabio &usbotg1 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_usb_otg1_id>;
 dr_mode = "otg";
 srp-disable;
 hnp-disable;
 adp-disable;
 status = "okay";
}; */
&usbotg1 {
 dr_mode = "host";
 disable-over-current;
 status = "okay";
};
&usbotg2 {
 dr_mode = "host";
 disable-over-current;
 status = "okay";
};
&usbphy1 {
 fsl,tx-d-cal = <106>;
};
&usbphy2 {
 fsl,tx-d-cal = <106>;
};
&usdhc1 {
 pinctrl-names = "default", "state_100mhz", "state_200mhz";
 pinctrl-0 = <&pinctrl_usdhc1>;
 pinctrl-1 = <&pinctrl_usdhc1_100mhz>;
 pinctrl-2 = <&pinctrl_usdhc1_200mhz>;
 cd-gpios = <&gpio1 19 GPIO_ACTIVE_LOW>;
 keep-power-in-suspend;
 enable-sdio-wakeup;
 vmmc-supply = <®_sd1_vmmc>;
 status = "okay";
};
&usdhc2 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_usdhc2>;
 non-removable;
 status = "okay";
};
&wdog1 {
 pinctrl-names = "default";
pinctrl-0 = <&pinctrl_wdog>;
 fsl,ext-reset-output;
};
&adc1 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_adc1>;
 vref-supply = <®_vref_adc>;
 num-channels = <10>;
 status = "okay";
};
there is no way to set output value 1 to the GPIO4_IO20 via dts.
Best regards
igor
ok
do you know an example where I can keep some source code to speed up my application where I can set some GPIO?
thanks
Hi Fabio
one can look at linux gpio dts documentation
fsl-imx-gpio.txt\gpio\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel
fsl,imx6ul-pinctrl.txt\pinctrl\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel
so gpio pad settings can be configured in dts file.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi These links are not working
Thanks Igor,
I will try :-)
Fabio