Hello,
I'm working with the imx6ullevk board running freescale Yocto.
After some experiments with custom SW application which accesses GPIO via mapped memory board fails to boot.
It was working fine and then was left for some time (weekend) powered but no custom SW was running.
Today after restart nothing is displayed to the serial debug console and moreover it looks that DDR memory chip becomes hot.
Is there any diagnostics I can do or is such failure recoverable at all?
Regards, Aleksej Kolga
Hi Aleksej
ddr chips can be tested with ddr test tool
i.MX6/7 DDR Stress Test Tool V2.80
As for imx6ullevk board boot, one can program new image
using Demo Images from below link, use Linux Guide from Linux documentation package
To avoid issues, first recommended to disconnect all cables from board, wait some time,
connect power cable, power-up board, then attach other cables. Avoid to apply external signals
to unpowered board.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Actually, the UART serial port is not accessible, neither PuTTY or screen on Linux cannot connect.
I mean, no output is printed to the serial console at all. And DDR test tool says "ERROR: Can't open USB device!!!"
I'm trying to boot from the original SD card which came with the EVK. Is has not been modified, so should contain valid boot image.
On the board itself after powering it on, green LED is lit, but orange is flashing just for a moment and then always OFF.
DDR chip becomes very hot after few seconds.
Regards, Aleksej
Hi Aleksej
in general one can check hardware using guidelines in
Hardware Development Guide for the i.MX 6ULL Applications Processor
https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf
NXP return service:
Returns and Warranty Information|NXP
Best regards
igor