IMX6ULL-EVK Tamper Pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL-EVK Tamper Pins

1,515 Views
imme_jakobeit
Contributor I

I would like to test the function of the tamper pins on this board. My Project is about detecting a tamper attempt on a case which is going to be built around the board. For my prototype I wanted to show that if I cut a wire (which is attached to the board) the IMX6-Board can detect this.

Is this possible?

If yes, where do I connect the wire?

Can I connect the wire to the tamper Pins (e.g. SNVS_Tamper0 and SNVS_Tamper1)? 

Which registers do I have to enable?

Thanks for the help.

Labels (1)
0 Kudos
Reply
1 Reply

1,302 Views
igorpadykov
NXP Employee
NXP Employee

Hi Imme

 

there is no tamper pin function in i.MX6ULL. TAMPER0-9 are used as GPIO.

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply