Our Customised design using IMX6ULL we are facing the issue in SD boot and eMMc boot because we are not using switch for BT_CFG2[3] to change Sd or eMMc boot.
We followed the NXP EVK boot configuration resistor setting same in our design.
Following are the Queries:
Please find the attached image which have marked the BT_CFG2[3]
Thanks in advance,
Rameshkumar
Hi ramesh
ROM basically is the same for both IMX6UL and IMX6ULL processors.
One can try to find reason of such behaviour reading with jtag SRC_SBMR1,2 registers.
>Can be possible to change only Software code level(uboot) to make this board work SD/eMMC
>without hardware modification?
no, as boot configuration is sampled by ROM from boot pins.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------