Hello,
I encounter an audio recording problem on our IMX6UL board.
Code is base on L3.14.52_1.1.0 BSP, but the board uses SAI3, it's different from IMX6ULEVK which uses SAI2.
I refer Linux user guide section 7.3.5 Audio recording and use ALSA "arecord" utility to test.
But can't record successfully.
We find the value of SAI3 0x20300A0 register(I2S3_RDRn) is no change when recording,
But we can measure BCLK, LR CLK, or Data signal.
I will be appreciated if someone can help to fix the issue.
Thanks.
P.S. IMX6ULEVK with L4.1.15_1.0.0 or L4.1.15_1.1.0 demo image also can't recoard.
Some DTS configuration is modified as below.
IMX6UL.dtsi:
sai3: sai@02030000 {
compatible = "fsl,imx6ul-sai";
reg = <0x02030000 0x4000>;
interrupts = <GIC_SPI 24 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_SAI3_IPG>,
<&clks IMX6UL_CLK_SAI3>,
<&clks 0>, <&clks 0>;
clock-names = "bus", "mclk1", "mclk2", "mclk3";
dmas = <&sdma 39 25 0>,
<&sdma 40 25 0>;
dma-names = "rx", "tx";
status = "disabled";
};
IMX6UL-14x14-evk.dts:
sound {
compatible = "fsl,imx-audio-rt5672";
model = "rt5672-audio";
cpu-dai = <&sai3>;
audio-codec = <&codec>;
codec-master;
gpr = <&gpr>;
hp-det = <1 0>;
&sai3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai3>;
assigned-clocks = <&clks IMX6UL_CLK_SAI3_SEL>,
<&clks IMX6UL_CLK_SAI3>;
assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <0>, <24576000>;
status = "okay";
};
codec: rt5672@1c {
compatible = "rt5670";
reg = <0x1c>;
clocks = <&clks IMX6UL_CLK_SAI3>;
clock-names = "mclk";
};