IMX6UL SAI(I2S SLAVE MODE)BCLK QUESTION

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL SAI(I2S SLAVE MODE)BCLK QUESTION

622 Views
strive
Contributor I

Dear  Expert:

About IMX6G3CVM05AA,about the SAI(I2S SLAVE MODE) ,I have the question below,please help,thanks

In the i.mx6ul datasheet,there is a description below:

pastedImage_1.pngpastedImage_2.png

question:

(1)how long is the "S11" in the Figure 62 above?

(2)how long is the "4 x tsys" in the table73?

         "S11" is is figure 62,that is slave mode.

         "S11" is the table73,that is Master mode

          which is correct?

BRs

Tom

Labels (1)
0 Kudos
Reply
1 Reply

480 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tom

one can look at i.MX7D SAI specs (the same as i.MX6UL) in

sect.4.10.12 SAI/I2S switching specifications i.MX7D Datasheet

http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7DCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply