IMX6UL: Is it possible to fuse more than one SRK (public key)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL: Is it possible to fuse more than one SRK (public key)?

Jump to solution
846 Views
sikumar3
Contributor III

Hi,

We are planning to use two separate keys one for development nodes and another one for production nodes.

 

Is it possible to fuse more than one SRK?

Is it possible to add additional public key after the Fuse is closed?

 

Regards,

Siva

0 Kudos
1 Solution
818 Views
sikumar3
Contributor III

Thanks Yuri for the quick clarification!

View solution in original post

4 Replies
839 Views
Yuri
NXP Employee
NXP Employee

@sikumar3 

Hello,

    All four SRKs (SRK table) should be flashed, since HAB evaluates the SRK table,
included in the signature, by hashing it and comparing the result to the SRK fuse
values.

Regards,
Yuri.

0 Kudos
834 Views
sikumar3
Contributor III

Hi Yuri,

 

Thanks for the response!

If only one SRK is fused and the fuse is closed, will I be able to add additional SRK in this scenario?

0 Kudos
824 Views
Yuri
NXP Employee
NXP Employee

@sikumar3 

If only one SRK is fused and the fuse is closed, will I be able to add additional SRK in this scenario?

No.

0 Kudos
819 Views
sikumar3
Contributor III

Thanks Yuri for the quick clarification!