IMX6UL: Dual uboot for recovery purpose

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL: Dual uboot for recovery purpose

Jump to solution
887 Views
sikumar3
Contributor III

Hi,

We are using IMX6UL EVK based board and eMMC is our primary boot device.

eMMC is partitioned as below:

mmcblk1boot0  --> uboot

mmcblk1boot1  --> empty

mmcblk1p2    --> active image (kernel, rootfs)

mmcblkp3       --> recovery image(kernel, rootfs)

we wanted to use one more recovery uboot binary either in the same eMMC or in a different storage device (SPI NOR FLASH, EEPROM etc).

 

If the primary boot device fails, NXP boot ROM will try to boot any other boot device?

 

Regards,

Siva

0 Kudos
Reply
1 Solution
880 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

No, it will not. For the boot mode set different flashes are different.

boot device.PNG

View solution in original post

0 Kudos
Reply
3 Replies
881 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

No, it will not. For the boot mode set different flashes are different.

boot device.PNG

0 Kudos
Reply
874 Views
sikumar3
Contributor III

Hi,

Thanks for the quick clarification!

864 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You are welcome. Have a nice day.

0 Kudos
Reply