你好:我们在测试IMX6UL的上电的时候发现,VDD_SOC_CAP和VDD_SARM_CAP的上电内部LDO对其输入电源VDD_SOC_IN有较大冲击,特别是VDD_SOC_CAP能把VDD_SOC_IN拉下。
(1)在规格书中看到PMU_REG_CORE寄存器中的RAMP_RATE和PMU_MISC2n寄存器中的REG2_STEP_TIME和REG0_STEP_TIME这些寄存器能调整内部LDO的上电斜率,但实际上写这些寄存器测试波形,不起效果。
(2)规格书中table11的comment中有VDD_SOC_IN must be 125mv higher than the LDO output Set point的要求,由于这个上电冲击电流,导致上电VDD_SOC_IN被拉下的瞬间与DD_SOC_CAP的压差达不到125mv的要求
请问:
(1)能否通过配置寄存器的方法来降低VDD_SOC_CAP和VDD_SARM_CAP的LDO冲击电流;怎么操作
(2)在上电阶段由于LDO打开冲击电流导致VDD_SOC_IN被拉下的瞬间与DD_SOC_CAP之间压差不能达到125mv的情况,是否被允许?是否会导致系统稳定性问题。这个125mv的压差是否是对稳定后的电源的要求?
The datasheet says run mode. not power up Sequence.
It is related to the DVFS settings.
Power up Sequence has restrict in another chapter in the datasheet.
谢谢回复,那么,到底如何修改寄存器才能让这个LDO的上电斜率变缓呢?
请NXP的技术支持帮忙回复下,谢谢
请问你这里用的板子是你们自己设计的板子吗?板子上跑的什么系统?
(1)这个板子是我们自己画的,其他功能都正常,高低温测试也没有问题。我们也测试了一块外购的开发板,这个LDO拉低输入电源的问题也同样存在。 而且在输入端增加电容收效甚微,只有去掉LDO输入的22uf电容才能消除这个冲击电流,手册上明确需要这个22uf的电容。
(2)文件系统是rootfs根文件系统,内核是linux4.15