IMX6Solo and Dual surface load capacity .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Solo and Dual surface load capacity .

ソリューションへジャンプ
1,135件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer has below question.

Please advice me.

iMX6 Solo and Dual surface on heat radiation sheet and place the heat sink on .

Would you please disclose the load capacity of the iMX6.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,067件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

heat spreading and dissipation capabilities are described

in AN4579 i.MX 6 Series Thermal Management Guidelines,

in particular pay attention to Appendix D Heat Sink Selection

http://cache.nxp.com/files/32bit/doc/app_note/AN4579.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,068件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

heat spreading and dissipation capabilities are described

in AN4579 i.MX 6 Series Thermal Management Guidelines,

in particular pay attention to Appendix D Heat Sink Selection

http://cache.nxp.com/files/32bit/doc/app_note/AN4579.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,067件の閲覧回数
takashitakahash
Contributor III

Dear Igor.

Thank you for your replay.

Although I got answer that there is no provision of the pressure load on the package of IMX6 in the previous question,

In simulation to i.MX6 compressive load 100N (10kg), 300N (30kg) and 1000N(100Kg) ,Can you determine no problem level in practical use ?

(I would like you to look at the presence or absence of occurrence of stress to the internal circuit as a determination material)

Thank you ,

Best Regards.

T.Takahashi

0 件の賞賛
返信