Hi everyone,
I'm trying to have both the m4 and a9 boot from ddr since my custom board (based on the imx6sx-sabresd) doesn't have the qspi flash.
If I directly boot linux (kernel version 3.10.53) on the a9, without removing the reset on the m4 everything works just fine.
Following this guide: How to Run the MQX™ RTOS on Various RAM Memories for i.MX 6SoloX I was able to load the "hello" example of the MQX RTOS at the address 0x80000000 and then run it through "bootaux 0x80000000" using u-boot. The m4 core is working fine since I am able to see the "Hello World" from the m4 console being printed.
However if I try to boot linux after booting the M4 core, I get stuck at:
Kernel image @ 0x81800000 [ 0x000000 - 0x54a908 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300e893
switch to ldo_bypass mode!
Starting kernel ...
And nothing happens later.
I also tried appending "uart_from_osc" in the mmcargs variable in u-boot, but still nothing changes.
Has anyone experienced the same problem?
Thanks for your help.
解決済! 解決策の投稿を見る。
I actually solved this.
The .dts file in the kernel version 3.10.53 doesn't include some necessary modifications needed to boot both the a9 and m4.
I just added this file imx6sx-sdb-m4.dts to my board .dts file. Even if it is for the 3.14.58 kernel version, it worked just fine for me.
The "uart_from_osc" command will make sure that the m4 console won't get corrupted when both the a9 and m4 are running.
Hope this will help you.
I have a similar problem , I have a kernel panic.
Any help?
I actually solved this.
The .dts file in the kernel version 3.10.53 doesn't include some necessary modifications needed to boot both the a9 and m4.
I just added this file imx6sx-sdb-m4.dts to my board .dts file. Even if it is for the 3.14.58 kernel version, it worked just fine for me.
The "uart_from_osc" command will make sure that the m4 console won't get corrupted when both the a9 and m4 are running.
Hope this will help you.
Hi Alan,
even i have same problem kernel locks after loading m4 when i try to boot
I am using IMX7D board
have imx7d-sdb.dts file .. where exactly i have to copy ..i copied to my board SDCARD but still same response .
Could you please tell me where i have to copy
Thanks in advance
problem solved by doing this:
$ setenv fdt_file imx7d-sdb-m4.dtb
$ save
Thanks, it works!