Hi all,
i'm struggling with my IMX6SX based platform.
I'm using Yocto with kernel 3.14.28+g91cf351.
On my device I monted a eMMC 4.41 compliance and I'm able to make it working with DDR and 4 bits data bus.
I'm trying to enable 8bit data bus but I found out that the kernel fails to request that type of bus and switch back automatically to 4 bits.
Into dts bus-width is correctly set to 8.
I found out that the kernel drvier receive error -84 into data.err when try top read CSD data using function mmc_send_cxd_data (code in mmc_ops.c) called by mmc_init_card (in mmc.c) where the DDR wide bus activiation is performed (around line 1642).
Are there known bugs on this matter?
已解决! 转到解答。
Hi LP
is it working in 8 bit non-ddr mode, are you able to boot in this
mode and successfully work in uboot ? One can check waveforms of data lines
with oscilloscope and try this part on i.MX6SX Sabre SD board using U4 eMMC Footprint.
Note for ddr mode may be necessary to tweak MMC_DLL_DLY values please check
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
What I'm seeing is that:
what bsp used in the case, could you try to reproduce issue with
nxp official L3.14.28 bsp on i.MX6SX Sabre SD board
linux-2.6-imx.git - Freescale i.MX Linux Tree
Best regards
igor
Hi Igor,
I set fuses to start at 1 bit. So U-Boot uses 8 bit mode, but I reall don't know if it uses DDR mode, I think it is.
All is loaded correctly and kernel is loaded and launched, but It continuously fails to set up DDR 8 bit mode, wit the error I reported.
I cannot check different BOOT configuration, I'm on my final board design and only fuses are available.
It smell like A9 communication with eMMC is failing for something like timeout, but, as you probabl knows, it is hard to debug the kernel....
Hi LP
could you try latest L4.1.15 kernel
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/?h=imx_4.1.15_1.0.0_ga
Best regards
igor