IMX6SX RPMSG BOOT ISSUE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SX RPMSG BOOT ISSUE

654 Views
2548903578
Contributor III

  When I use the imx6sx development board to use RPMSG to realize dual-core communication, I found that when I first start the M4 core and then start the A9 core, there is no problem with the dual-core communication. When I start A9 and then M4, there is no response when I load the corresponding .ko file. I saw in an article that it is possible to start A9 first and then realize dual-core communication, so I want to ask whether the dual-core communication of imx6sx can be started by the second method.

  The screenshot is the implementation method of the article I am looking for. This article is to start A9 first, then start M4, and finally realize dual-core communication.

QQ截图20201013103118.png

 

0 Kudos
Reply
2 Replies

638 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

634 Views
2548903578
Contributor III

Hi!

I saw the content about RPMSG in Chapter 5. I think this chapter is to start M4 first and then start A9 core. Can imx6sx start A9 first and then M4?QQ截图20201013161712.png

0 Kudos
Reply