IMX6SX LCDIF 8bits

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6SX LCDIF 8bits

1,851 次查看
LPs
Contributor III

Hi all,

  due to a very slow 320x240 lcd (6,5 MHZ with 24bit parallel) I'm trying to configure LCDIF device to use a 8bits bus wicth.

I changed the dtb as below:

&lcdif1 {

  pinctrl-names = "default";

  pinctrl-0 = <&pinctrl_lcdif_dat

      &pinctrl_lcdif_ctrl>;

// lcd-supply = <&reg_lcd_3v3>;

  display = <&display0>;

  status = "okay";

  display0: display {

  bits-per-pixel = <24>;

  bus-width = <8>;

  display-timings {

  native-mode = <&timing0>;

  timing0: timing0 {

  clock-frequency = <19500000>;

  hactive = <320>;

  vactive = <240>;

  hback-porch = <204>;

  hfront-porch = <60>;

  vback-porch = <18>;

  vfront-porch = <4>;

  hsync-len = <10>;

  vsync-len = <10>;

  hsync-active = <0>;

  vsync-active = <0>;

  de-active = <1>;

  pixelclk-active = <0>;

  };

  };

  };

};

The problem is that the kernel hangs!!!

I recompiled my kernel with early printk but it prints

Starting kernel...done, booting

But nothing more.

If I change the bus with to 16 or 24 the kernel starts.

What is the problem? What can I do to debug the 8 bit problem?

标记 (4)
0 项奖励
回复
2 回复数

1,481 次查看
davidtrinh
Contributor II

Hi,

If you look at the driver you will see that the 8 bits mode for LCDIF is not yet supported.  You have to modify the driver to have it work for you.

Also, if you are using sources from the yocto distribution, This comment: // lcd-supply = <&reg_lcd_3v3>;

will make the driver to no working since it will break out of the initial process if the supply is not existed.

To sum up, to support 8 bits mode, modifying the device tree alone won't help much.

Good luck!

1,481 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello LPs,

Would you please share the diff so we can see what changes were made on the file? And also, would you please let us know why did you commented the LCD supply?

Regards,
Gustavo

0 项奖励
回复