IMX6SX ADC Resistive TouchScreen driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6SX ADC Resistive TouchScreen driver

2,305 次查看
LPs
Contributor III

Hi all,

  is a touchscreen linux driver available, that use the SoC ADC module instead of an external ADC?

Regards

标签 (4)
0 项奖励
回复
4 回复数

1,874 次查看
igorpadykov
NXP Employee
NXP Employee

Hi LP

i.MX6SX has ADC but it is not designed for touchscreen usage.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,874 次查看
LPs
Contributor III

Hi Igorpadykov,

   could you elaborate your answer, please?

Why isn't it designed for that porpose? What is the difference between the SoC ADC module and an external serial ADC?

Thanks

0 项奖励
回复

1,874 次查看
igorpadykov
NXP Employee
NXP Employee

please refer to Chapter 14 Analog-to-Digital Converter (ADC)

i.MX6SX Reference Manual (rev.0  2/2015) for additional info

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

~igor

0 项奖励
回复

1,874 次查看
LPs
Contributor III

Ok,

  due to the ADC module that cannot be used as GPIO.

Thanks

0 项奖励
回复