IMX6SLEVK lcd resolution kernel modify(240x320 -> 320x240)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SLEVK lcd resolution kernel modify(240x320 -> 320x240)

662 Views
chuyeonsoo
Contributor I

Dear,

I am trying to setup a custom display on a IMX6SLEVK and I am facing some problems.

In my board is equipped with a 240x320 resolution LCD. I want to modify the kernel of the resolution to 320x240 IMX6SLEVK. If you do need to resolve this issue, modify the kernel somewhere?

Best regards,

Chu

Labels (4)
Tags (3)
0 Kudos
2 Replies

422 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi chu yeonsoo,

Which BSP are you using?
Have a great day
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

422 Views
chuyeonsoo
Contributor I

Dear, Dan


BSP is being developed fsl-community-bsp-platform (daisy: branch). Also developed in the Yocto project.

In addition, I use the ili9341 lcd controller in our platform.


Have a nice day

Chu


0 Kudos