IMX6S can't read the peripheral Registers with UlinkPro and DS5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6S can't read the peripheral Registers with UlinkPro and DS5

519 Views
fschl
Contributor I

Hi! I want to bare metal debugg the cortex M4 on the IMX6S with the UlinkPro and DS5. It works good until i want to read the peripheral Registers. And it does not matter which peripheral i choose, the connection to the Board will be interrupted and a reset of the Board is necessary. But i can read the other Registers ( Core, System, FP ).

Is there any possibility to get an access to the peripheral Registers?

Thanks for your Help :smileyhappy:

Felix

0 Kudos
1 Reply

426 Views
igorpadykov
NXP Employee
NXP Employee

Hi Felix

please try attached script Setup_M4.ds

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos