IMX6Quad board using Network File System (NFS)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Quad board using Network File System (NFS)

2,101 次查看
jgn763
Contributor I

Hi All,

We're trying to boot Android Nougat (7.1) IMX6Quad board using Network File System (NFS)

After a lot of trail & errors, we reached to some point. Now kernel is loaded successfully, but it got stuck while loading init.

Booting has stopped with below error.


VFS: Mounted root (nfs filesystem) on device 0:17.
devtmpfs: mounted
Freeing unused kernel memory: 1024K (c1100000 - c1200000)
Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
CPU2: stopping
CPU: 2 PID: 0 Comm: swapper/2 Tainted: G W 4.1.15-dirty #2
Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)


Attached the complete log file for reference.

Please find the below configurations we're setting for network boot.

setenv ipaddr xx.xx.xx.68
setenv serverip xx.xx.xx.192
setenv nfsroot /srv/nfsandroid
setenv ip_dyn no
setenv bootfile zImage
setenv fdtfile imx6q-wandboard-revd1.dtb
setenv netargs 'setenv bootargs ${bootargs_base} console=${console},${baudrate} root=/dev/nfs rootwait rw ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp'
env save

Regards,
Saran

标签 (2)
标记 (2)
0 项奖励
回复
4 回复数

1,939 次查看
jimmychan
NXP TechSupport
NXP TechSupport

"Kernel panic - not syncing: No working init found. " Basically, this error means your Android filesystem has problem. please double check the Android system files are in your nfsroot.

0 项奖励
回复

1,939 次查看
jgn763
Contributor I

   Hi Jimmy,

We tried both the blogs and all the steps mentioned. We could not make the rootfs up. It is the same issue. Is there any freescale document to cross check? For nougat on NFS

Help would be very much appreciated.

Thanks in advance

Regards,

Saran

0 项奖励
回复

1,939 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,939 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励
回复