IMX6Qaud platform is unstable on Android 5.1.1 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Qaud platform is unstable on Android 5.1.1 BSP

1,403件の閲覧回数
mayqueen
Contributor IV

Hello~

As title, I find out it's not stable when I boot up on Android 5.1.1, it could boot up into the desktop first time, but when I reboot again, no boot success any more ( stock on the android animation screen), the logcat message as below:

W/linker  (  375): libGLESv1_CM.so: unused DT entry: type 0xff000000 arg 0xff000000

W/linker  (  375): libGLESv1_CM.so: unused DT entry: type 0xff000000 arg 0xff000000

W/linker  (  375): libGLESv1_CM.so: unused DT entry: type 0xff000000 arg 0xff000000

Can anybody help me, please?

Thank you!

ラベル(1)
タグ(1)
3 返答(返信)

1,252件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

I will test the newest SBP on my board and give you feedback.

1,252件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Do you design the board yourself or use the board from NXP?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,252件の閲覧回数
mayqueen
Contributor IV

I just use SABRESD-IMX6Q EVK board.......... I will use other board (Wandboard and Udoo board) to test after I back to China, but before that, I need some direction or comment, thank you! Because the customer doesn't agree a unstable product, right?

Thank you!

0 件の賞賛
返信