IMX6QP: Maximum supported DDR size

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6QP: Maximum supported DDR size

971 Views
kishorr
Contributor II

As per IMX6QP data sheet, the maximum supported DDR size is 3840MB. I would like to know if this is the max DDR that can be used with imx6qp.

Thanks

Kishor

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

832 Views
Yuri
NXP Employee
NXP Employee

Hello,

  let me remind, for 32-bit addresses 4GB is maximum address area.

But some address range should be left for peripherals.  

Regards,

Yuri.

0 Kudos
Reply

832 Views
kishorr
Contributor II

blockquote, div.yahoo_quoted { margin-left: 0 !important; border-left:1px #715FFA solid !important; padding-left:1ex !important; background-color:white !important; } Hi Yuri,Thank you If we would need to have 8gb, is it possible?

Does ARM V7-A CPU architecture provides a way ThanksKishor 

Sent from Yahoo Mail for iPhone

0 Kudos
Reply

832 Views
Yuri
NXP Employee
NXP Employee

Hello,

If 8gb means 8GBytes - I am afarid - we cannot support it under i.MX6.

Regards,

Yuri. 

0 Kudos
Reply

832 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kishor

this is defined by max. supported row/col parameters described

in sect.44.12.1 MMDC Core Control Register (MMDCx_MDCTL) i.MX6DQ Reference

Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply