IMX6QP Errata related problem question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6QP Errata related problem question

592 Views
Rayn_Jang
Contributor I

 

We are getting boot errors related to Errata ERR009624.

Booting error is output as below and LCD is not output.

The problem occurs in CPU Silicon Revision V1.1, and it works well in Silicon Revision V1.0.

Can you tell me if there is a patch code that works with CPU Silicon Revision V1.1 and V1.0?

 

Error Log Messages =====================================================

[ 12.039727] init: Starting service 'keystore'...
[ 12.040849] init: cannot find '/system/bin/rild', disabling 'ril-daemon'
[ 12.041015] init: Starting service 'zygote'...
[ 12.041703] init: Starting service 'gatekeeperd'...
[ 12.051618] init: Starting service 'perfprofd'...
[ 12.052422] init: Starting service 'magd'...
[ 12.258147] android_work: sent uevent USB_STATE=CONNECTED
[ 12.285786] configfs-gadget gadget: high-speed config #1: b
[ 12.291904] android_work: sent uevent USB_STATE=CONFIGURED
[ 12.706534] init: Service 'magd' (pid 270) exited with status 255
[ 13.264230] drivers/video/fbdev/mxc/ldb.c : ldb_disable
[ 13.264282] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000
[ 14.276377] imx-prg 21cd000.prg: wait for buffer ready timeout
[ 14.276894] drivers/video/fbdev/mxc/ldb.c : ldb_enable
[ 15.285237] imx-pre 21cb000.pre: timeout waiting for PRE to run out of problematic window for shadow update
[ 15.407529] init: Starting service 'bootanim'...
[ 16.405411] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 17.405335] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 18.405280] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 18.480366] random: nonblocking pool is initialized
[ 19.405291] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 20.405287] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 21.386198] capability: warning: `main' uses 32-bit capabilities (legacy support in use)
[ 21.405333] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 22.405310] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 23.405270] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0

=========================================================================

Best regards,

James.W

Labels (1)
0 Kudos
Reply
0 Replies