IMX6Q use 4GB DDR3 only CS0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q use 4GB DDR3 only CS0

671件の閲覧回数
yangruofei
Contributor I

    we use the ref design  DDR3 layout route of iMX6Q_SABRE_SDB_DESIGNFILES . but now we use four pcs  512Mb x16(1GB) DDR3 memery 。  we use the DDR stress tool to Calibration the DDR parameter and test . when we select 2GB to TEST , it test passed. and when use 3.84GB to test .  it will fail each cycle.  

      and we use the  DDR Calibration parameter to update u-boot, u-boot debug message will report 3.84GB(MAX sapce). but  when run into kernal and filesystem . it will be hang. could not operate normal .

please help me to fixed this issue.

タグ(2)
0 件の賞賛
1 返信

415件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yang

please check presentation describing DDR stress tool 

https://community.nxp.com/docs/DOC-331528

and attached 4GB example.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛