IMX6Q the clk of DDR3 when using fly-by topology (Very Urgent)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q the clk of DDR3 when using fly-by topology (Very Urgent)

786 Views
weivivien
Contributor I

hello,

We have a very urgent problem about iMX6Q and DDR3.

According to the design of IMX6Q reference design, it use four DDR chips with T-topology and use two pair of CLK(CLK0 CLK0# and CLK1 CLK1#) and one cs signal.

In our design, we have a special cross section of PCB, so we can't use T-topology, so we decide to use fly-by topology.

BUT, we have question ahout CLK and CS.

Could we still use 2 pair of clk and  ONE CS signal to monitor 4 chips of DDR3(just like the schematic of reference design in T-topology and add termination res).or we have to use 1 pair of clk and 1CS signal to control 4 DDR chips

thank you very much!

vivien

Labels (3)
0 Kudos
3 Replies

560 Views
igorpadykov
NXP Employee
NXP Employee

Hi vivien

in that case recommended  to use 1 pair of clk and 1CS signal to control 4 DDR chips

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

560 Views
weivivien
Contributor I

Thank you very much for your reply!

But our BSP bootloader of DDR is writed for 2 pair of clk signals to control 4 DDR chips, can we still use 2 pair of CLK in fly-by topology?

Because it's an challenge for us to edit the BSP bootloader. 

Best regards
vivien

0 Kudos

560 Views
weivivien
Contributor I

Thank you very much for your reply!

But now we can't understand why their is two CLK for 4 DDR chips in T-topology and just one CS signal.

0 Kudos