IMX6Q - initcall sequence 8ffb54a4 failed at call 17803305 (err=-22)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q - initcall sequence 8ffb54a4 failed at call 17803305 (err=-22)

1,214 次查看
robertZ
Contributor II

Hi,

I have an unusual problem.

I have a device that works as intended. However, from time to time - Regardless of the conditions (temperature, humidity, some sequence), the device does not start and after connecting the terminal there is only a message:

 

CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 28C
Reset cause: POR
I2C: ready
DRAM: 2 GiB
PMIC: PFUZE100 ID=0x10
Not supported, id=12
initcall sequence 8ffb54a4 failed at call 17803305 (err=-22)
### ERROR ### Please RESET the board ###


The fix for the problem is that if you take out the SD card with the system and put it back in, everything returns to proper functioning.

Has anyone encountered this problem and how can it be fixed?

 

标签 (2)
0 项奖励
回复
1 回复

1,197 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
if you take out the SD card with the system and put it back in, everything returns to proper functioning.
=>There are chances of issue in detection of the SD card. 
Please check the same in the Hardware that everytime the SD card is being detected properly or not. 
 
Thanks & Regards
Sanket Parekh
0 项奖励
回复