Hi, I am writing a driver to use IMX6Q to receive image data from a CMOS chip(ev76c560), with 1280*1024 pixels, and the pixel clock is 114 MHz. I can read data from the chip pins by using oscilloscope, but I can't read data from ipu. Is the width of the image data too big, or the frequency of the pixel clock too high?