IMX6Q Video freeze at high temperature.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q Video freeze at high temperature.

626件の閲覧回数
agnel_terry
Contributor III

HI

I have a custom board with Imx6Q automative part,

I am running a video in loop , inside a temperature chamber at 60degreeC  , when the processor temperature reaches  above  95C the video freeze with Gstreamer crash ,

The processor is not locking up, I can rerun the script to play the video without power cycle but again when the temperature reaches near 95C the video Freeze.

If i run the video in ambient and if the processor temperature is maintained bellow 90 degree C ,  The video run fine without any issue,

Is there any suggestion or reason why the video freeze at this temperature.

Thanks and Regards

Terry

 

 

 

 

 

 

0 件の賞賛
3 返答(返信)

584件の閲覧回数
agnel_terry
Contributor III

Hi Weidong,

Is there a reason why we need to reduce the temp limit from 125 to 115 ?

 

Thanks and Regards

Terry

0 件の賞賛

616件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

The driver of the temperature monitor is imx_thermal.c, you can adjust the upper limit temperature to 115°C, and then test it again.

Have a nice day!

B.R,

Weidong

0 件の賞賛

611件の閲覧回数
agnel_terry
Contributor III

Thank you Weidong, I hope you are taking about the passive trip limit? 

however the temp reading I am getting from the sysfs

/sys/class/thermal_zone/temp gives 95 degree C and still it Freeze . 

0 件の賞賛