HI
I have a custom board with Imx6Q automative part,
I am running a video in loop , inside a temperature chamber at 60degreeC , when the processor temperature reaches above 95C the video freeze with Gstreamer crash ,
The processor is not locking up, I can rerun the script to play the video without power cycle but again when the temperature reaches near 95C the video Freeze.
If i run the video in ambient and if the processor temperature is maintained bellow 90 degree C , The video run fine without any issue,
Is there any suggestion or reason why the video freeze at this temperature.
Thanks and Regards
Terry