IMX6Q UART work with RS485 function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6Q UART work with RS485 function

跳至解决方案
2,386 次查看
lifusong
Contributor IV

Dear sir.

    we board have four uart work with RS485 (UART1 UART2 UART3 UART5)  kernel 3.14.52

pastedImage_1.png

we modify the file : driver/tty/serial/imx.c 

the uart look seem work ok when only one uart work

but more than one rs485 uart work together, will can't read data when uart A is r/w data during B is r/w data.

how to fix.

Had Fix issue.

   the point is tx chang to rx, must wait tx send data complete.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,169 次查看
lifusong
Contributor IV

Hi sir.

  thanks for your replay.

  we had fix this issue.

   the point is tx chang to rx, must wait tx send data complete.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,169 次查看
igorpadykov
NXP Employee
NXP Employee

Hi li

one can check suggestions provided on

[imx6] RS485 could be supported on Imx6 series ?  

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,170 次查看
lifusong
Contributor IV

Hi sir.

  thanks for your replay.

  we had fix this issue.

   the point is tx chang to rx, must wait tx send data complete.

0 项奖励
回复