IMX6Q - TVP5150 Support - BT656

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q - TVP5150 Support - BT656

ソリューションへジャンプ
2,315件の閲覧回数
patrickmccleary
Contributor II

Hello Everybody.

My first post on the i.MX Community forum! Anyway, I'm trying to incorporate a composite video input into the IMX6Q using TI's TVP5150 (BT656 NTSC) through the parallel camera interface (CSI0). I've got the TVP5150 kernel driver talking to the chip through the i2c bus but I'm not sure how to register it with v4l2. I'm pretty new to the linux kernel and v4l2 so any help or information would be greatly appreciated. Thanks!

I've also attached my board schematic to this post. If anyone would like the gerbers let me know.

-Pat

ラベル(4)
タグ(2)
0 件の賞賛
1 解決策
927件の閲覧回数
patrickmccleary
Contributor II

Hello Jimmy. My solution is to use the ADV7180 instead of the TVP5150AM1 as the FSL specific v4l2 kernel drivers support it out of the box.

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
927件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think you can read the linux BSP porting guide for more information about porting a camera/video input.

The document is i.MX_6Dual6Quad_BSP_Porting_Guide.pdf in the Linux BSP bundle.

you can download it from here:

i.MX 6 Series Software and Development Tool Resources Product Summary Page

0 件の賞賛
928件の閲覧回数
patrickmccleary
Contributor II

Hello Jimmy. My solution is to use the ADV7180 instead of the TVP5150AM1 as the FSL specific v4l2 kernel drivers support it out of the box.

0 件の賞賛